ROBINAIR
Founded in 1956, Robinair, a brand of Bosch Automotive Service Solutions, specialises in air conditioning & refrigeration equipment and tools. Headquartered in Warren, Michigan, USA, the brand has been benefitting HVAC, automotive and refrigeration technicians. Read More
Filter
HVAC and Refrigeration
Fleet and Vehicle Maintenance
Pneumatics
Lab Supplies
Plumbing
HVAC and Refrigeration Filter
A/C RefrigerationView all
A/C Refrigeration Accessories Refrigerant Evacuation Pumps VacuMaster vacuum pumps featuring a dual-stage offset rotary vane design for moisture removal and Sure-Grip handle for job-site portability; ideal for HVAC operations. Available in 3 and 8 CFM displacement variants
Refrigerant Recovery Cylinders Refrigerant Recovery Systems Suitable for recovering medium- and high-pressure refrigerants from HVAC equipment. Feature a high-pressure cut-out switch providing automatic operation and an oil-less compressor to circulate the fluids efficiently within the components
Refrigeration Access Valves
About Robinair
Robinair's extensive catalogue includes AC fittings & adapters, vacuum pumps, flushing kits, hoses, couplers, thermometers and leak detection equipment, as well as AC recovery, recycling & recharging units. The brand's vacuum pumps are engineered specifically for air conditioners and refrigerators to create a partial vacuum by removing air & moisture from the sealed system. These pumps come equipped with two-stage offset rotary vanes for powerful & quiet operation and finned surfaces for faster heat dissipation. Robinair also manufactures portable refrigerant recovery machine that is useful for removing refrigerants from HVAC systems. It is capable of removing liquid and vapour refrigerants (CFC, HFC, HCFC & R-410 A). This refrigerant recovery machine features a high-efficiency cross-flow design, an oil-less compressor and a high-pressure safety shut-off switch to withstand rugged use even in extreme weather conditions.
Things To Consider
Cross-Reference Alternatives
Robinair's part numbers often cross-reference to various YELLOW JACKETS and Bacharach products. So if you're looking for Robinair products that are either obsolete or out of stock, chances are we have equivalent items available.
Shipping
These Robinair products range from small to large sizes. They may require careful packaging as some items might get damaged while shipping. Hence, these items are delivered by courier shipment and air freight for minimum downtime.
Major Trade Names
DiscovR Refrigerant Identifier
Robinair DiscovR refrigerant identifier provides a fast, easy and accurate means to determine purity in refrigeration systems. It has 'Pass' and 'Fail' lights to notify users whether the system has en...Read more
VacuMaster Vacuum Pumps
The brand's VacuMaster vacuum pumps have a 2-stage rotary vane design for maximum moisture removal and reduced evacuation time. They have an angled oil drain valve at the bottom for faster and complet...Read more
Air Vac
Robinair Air Vac is a venturi-type vacuum pump (powered by compressed air) designed for mobile air conditioning service. It requires little maintenance because there are no moving parts, which means t...Read more
Frequently Asked Questions
How to maintain Robinair vacuum pumps?
- Replace the oil consistently to ensure the smooth operation of the pump.
- Clean the intake filter of the pump from accumulated dirt & debris.
- Clean the intake & outlet ports of the pump to ensure smooth flow of the refrigerant from the refrigeration system.
How to set up Robinair refrigerant recovery machines?
- Place the machine on a stable surface and install a clean filter screen or filter / dryer to the inlet fitting.
- Connect a hose from the liquid port of the recovery cylinder to the outlet fitting on the unit.
- Connect another hose from the outlet port of a manifold gauge set to the inlet fitting on the unit through the filter / dryer.
- Connect a hose from the selected system's liquid side to the liquid side of the manifold gauge set.
- Connect another hose from the system's vapour side to the vapour side of the manifold gauge set.
- Seal all the inlet & outlet valves and place the cylinder on a weighing scale to prevent overfilling.
What is the benefit of push / pull procedure in the brand's recovery machines?
Push / pull procedure in refrigerant recovery machines recovers refrigerants from large systems containing bulk liquids (over 15 lb).