YELLOW JACKET Evacuation Vacuum Pumps
Yellow Jacket vacuum pumps are mechanical devices suitable for removing gas and air molecules from a sealed area. Vacuum pumps can be used in a variety of industries and applications to remove air and gas molecules from a process, comprising the food and beverage industry, semiconductor and ele...ctronics industry, medical, woodworking and more. These vacuum pumps come in dry or wet variants, depending on the media passed through them.Read more
Style | Model | Amps AC | Body Material | Displacement | Inlet Port Size | Oil Capacity | Overall Length | Price (ex. VAT) | |
---|---|---|---|---|---|---|---|---|---|
A | 93600 | - | Aluminum | 7.0 cfm | 1/4" and 3/8" Flare | 28 oz. | 16.25" | €1,014.41 | |
B | 93580 | 6.2 | Metal | 8.0 cfm | 1/4" and 1/2" Flare | 32 oz. | 16.75" | - | RFQ
|
C | 93590 | 10.0 | Aluminum | 11.1 cfm | 1/4" and 1/2" Flare | 44 oz. | 17.5" | - | RFQ
|
Working Mechanism
- Yellow Jacket vacuum pump's primary function is to adjust the pressure in a confined space to produce a complete or partial vacuum either chemically or mechanically. The pressure will always try to balance across attached regions as gas molecules flow from high to low, filling the whole area of that volume.
- Thus, if a new low-pressure space is introduced, gas will naturally flow from the high-pressure area to the new area having low-pressure.
- Notice this vacuum process is created not by ?sucking? gases but by forcing molecules.
- Vacuum pumps effectively move gas molecules from one area to the next to create a vacuum by changing high and low-pressure states.
Features
- Yellow Jacket vacuum pumps have heavy-duty bearings & rotors and in-built cooling fins to cool the pump, improving performance.
- They feature a broad mouth oil reservoir port for comfortable, cleaner filling and a large brass oil drain for easy admission to rapid oil changes.
- These vacuum pumps have an isolation valve that permits for oil changes without losing vacuum in the unit and features a gas ballast valve that keeps the oil uninfected during the evacuation of a wet system.
- They come with a suitable shoulder strap for effortless transport over long stretches with in-built mount points.
- They come with an inner intake check valve that stops oil back up into the unit during a power loss.
- These Yellow Jacket vacuum pumps feature heavy-duty steel handles that provide comfortable carrying and a lifting hook for lifting pumps to rooftops.
Frequently Asked Questions
How do 2 stage vacuum pumps differ from 1 stage vacuum pumps?
A two-stage vacuum pump has two rotors and vanes. The first stage creates a vacuum and the second stage cleans the system, directing to a deeper ultimate vacuum level. As an outcome, two-stage pumps can deliver a deeper vacuum than single-stage pumps.
What do we mean by CFM in a vacuum pump?
CFM or Cubic Feet per Minute is the measurement of air flowing through a vacuum system.
How do we choose a vacuum pump?
While choosing a vacuum pump, users should consider factors, such as vacuum level & pumping speed, process or application impact on the pump and impact of the pump on the process or application. Users should also keep a check on maintenance costs associated with the pump.
Which type of oil is used for the vacuum pump?
The oil utilised in a large rotary piston vacuum pump is a mineral oil that has been through a distillation process to decrease its vapour pressure.
We are here to help!
Looking for a part not listed here?
Explore More
- Biohazard Waste Cans
- Heat Gun Accessories
- Bus Drop and Tray Cable
- Planes and Shaving Tools
- Laboratory Tongs and Forceps
- Disposable and Chemical Resistant Clothing
- Machining Supplies
- Generators
- Solenoid Valves and Coils
- Outdoor LED Light Fixtures
- BRADY Arc Flash Protection Label
- DIXON Springs
- HOFFMAN Current Transformer Cabinets
- THOMAS & BETTS KN14 Series Wire Disconnects
- EATON LV AutoVAR 300 Series Capacitor Banks
- MARTIN SPROCKET P1 Series MST Bushings
- APPROVED VENDOR Hydraulic Spin-on Filters
- DAYTON Combination Belt and Bench Grinders
- BALDOR / DODGE Split Tire, 40HCBM, Elastomeric Couplings
- WINSMITH SE Encore Series, E26 Size, MDJS Single Reduction Speed Reducers